2024-06-03 8:44 PM - edited 2024-06-16 7:38 PM
(address : 0x00- 0x0F) 00 00 00 00 00 00 00 ff 00 00 00 00 00 00 00 33 |........ .......3
(address : 0x10- 0x1F) 0f 86 6f 21 a0 22 20 27 1b a8 70 73 c0 00 90 00 |..o!." ' ..ps....
(address : 0x20- 0x2F) 27 05 40 00 0a 82 00 ff 00 0a 00 fe 00 3e 00 20 |'.@..... .....>.
(address : 0x30- 0x3F) 2a 25 01 78 00 00 00 00 15 00 d6 60 00 00 00 00 |*%.x.... ...`....
Thank you and best regards,
Bruce
2024-07-17 5:11 AM
you mention to use click interrupt and initial interrupt respectively.
In your configuration CTRL_REG3 (22h) = 40h --> this means that only IA1 interrupt is enabled while Click interrupt on INT1 is disabled.
I don't know what you mean for "initial" interrupt or which function you are using to get interrupt after 120 samples. My suggestion is to review sensor configuration according to your use case.