Skip to main content
Associate II
July 24, 2024
Question

STUSB4700 USB-C Power sourcing on a Slave device

  • July 24, 2024
  • 0 replies
  • 581 views

Hi,

I'm beginner in USB-C and USB_PD some things are not clear for me.

We developing a device which is a USB SLAVE Device - not HOST (Virtual comport device - datalogging to a notebook)

This device has a large battery, so we want to charge the notebook from this device. 

We want to keep things simple and use the STUSB4700 to enable up to 100W charging power.

Can the device supply charge power and still work as USB slave device?

Can the attached circuit work?

Regards

Falko

 

PS Forum Software:

> The following labels are not available here: USB-PD

Why can't i use label "USB-PD" ? Othe people was using it?

 

 

This topic has been closed for replies.