Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't load code on STEVAL-IDB011V1 by Keil

Hello.I'm using STEVAL-IDB011V1. From the BlueNRG-LP Navigator, I can load the examples on the board. But when I'm using the Keil, it says "SWD/JTAG Communication Failure".On the options for target in the tab "Device" the device is BlueNRG-355, and t...

Resolved! BlueNRG-2 maximum SPI clock

I am currently using a X-NUCLEO-BNRG2A1 to experiment with the BlueNRG-2. I initially set the SPI rate to 1.25 Mbit/s, but later noticed in the BlueNRG-2 documentation that the maximum SPI rate is 1Mbit/s. My question is how strict is this SPI rate l...

BPaik by Senior
  • 1688 Views
  • 3 replies
  • 0 kudos

Resolved! BlueNRG firmware version questions

I am currently using the X-NUCLEO-BNRG2A1 to experiment with the BlueNRG-2. Using the getBlueNRGVersion function, I see that the hardware version is 0x12 and the firmware version is 0x2211 and had some questions on how to interpret this:I believe the...

BPaik by Senior
  • 1634 Views
  • 4 replies
  • 0 kudos

x-cube ble stack on FreeRTOS

Hi ST,I had a question in regards to the x-cube BLE stack.While looking at the stack for the BlueNRG-M2SA I noticed that the BLE functionality (MX_BlueNRG_2_Process) was running in the MAIN inside of a while 1 loopMy question though, our system is ru...

KShar.4 by Associate II
  • 1316 Views
  • 1 replies
  • 2 kudos