User Activity

Hi.In PM0214 programming manual page 40 it says:On system reset, the vector table is fixed at address 0x00000000. Privileged software can write to the VTOR to relocate the vector table start address to a different memory location, in the range 0x0000...
Hello.I'm using STEVAL-IDB011V1. From the BlueNRG-LP Navigator, I can load the examples on the board. But when I'm using the Keil, it says "SWD/JTAG Communication Failure".On the options for target in the tab "Device" the device is BlueNRG-355, and t...