Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB4500 PDO profile doesn't change after setting.

Hi,Through some setup, I was able to access STUSB4500 using the GUI tool in STSW-STUSB002.After I set the second profile to 20V/5A, I connected a power supply with 5V/3A and 20V/3.25A PDO capability. But nothing changes and the voltage is unchanged a...

0693W000008wLMzQAM.png
BHan.1 by Associate II
  • 6084 Views
  • 3 replies
  • 0 kudos

S2-LP SMPS

Admittedly, this is going to be a challenge to answer since it appears what I'm doing is against the specification... but here it goes... hopefully someone at ST knows...Are most folks using these radios only in battery applications? I ask because t...

JMath.2 by Associate II
  • 1151 Views
  • 0 replies
  • 1 kudos

WB5x: HCI bugs over UART transport

Hi All,There seems to be multiple bugs in the HCI implementation for WB series chips.Are there any newer builds of this image where these are fixed?Setup: Using reference dongle from P-NUCLEO-WB55.stm32wb5x_FUS_fw.bin latest version - 1.1.2stm32wb5x_...

donpedro by Associate II
  • 2472 Views
  • 4 replies
  • 0 kudos