Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK V3 VCP "backpowers" board

Hello,I'm developing a board with the BlueNRG-M2 module. I'm also using an ST-LINK V3 with uVision to debug/program. I'm also using the VCP made available by the ST-LINK V3 for some good old fashioned printf telemetry. The VCP is connected through...

svcguy by Associate III
  • 3127 Views
  • 3 replies
  • 0 kudos

Getting extra bits in received message.

Trying to build a 433 MHz sniffer based on SDK example "SDK_Sniff_B.c". Im sniffing messages from TPMS sensor and get them on my PC with RTL-SDR. In the message parsed on PC I can read ID of sensor which goes right after sync word. With the help of U...

ATet.1 by Associate
  • 1196 Views
  • 1 replies
  • 1 kudos

I want to use hyperflash

I want to use hyperflash (S26KS512 or S26KL512) with stm32h723zet6 microcontroller.The memory has "Phase Shifted Clock" pins.What should I do with them? Connect to GND or VCC or Not Connected?Hyperbus interface (stm32) support 1.8v?

aoz.1 by Associate
  • 1133 Views
  • 2 replies
  • 0 kudos

BlueNRG paring problem

Hi ST community! I have been using BlueNRG for the next version of product in our company. I have a problem with pairing this module with phone. Once I paired with device, they are supposed to be connected even after phone restarts, but it is not the...

JKing.2 by Associate II
  • 945 Views
  • 0 replies
  • 0 kudos

RF channel frequency settings for S2LP

I am in the process of migrating from spirit1 to S2LP, I am stuck in the calibration of the frequency, before in spirit 1 it is mentioned in the datasheet of spirit1 via equation 3 fc=fbase+foffset+(fxo/2^15  ×CHSPACE)×CHNUMOn the other hand in the S...

H..10 by Associate II
  • 2206 Views
  • 4 replies
  • 0 kudos

Resolved! BlueNRG - Unable to advertise 128-bits services

I'm using a X-NUCLEO-BNRG2A1 shield on a NUCLEO-L476RG board.I am able to advertise 16-bits and 32-bits services using aci_gap_update_adv_data(), but trying with a 128-bits service always ends up with a "BAD PARAMETER" error. What am I missing? (I'm ...

paul19 by Associate III
  • 1483 Views
  • 5 replies
  • 0 kudos

Hi everyone, Here, Present am Working on TESEO-LIV3F gps interface am Trying to read GPRMC and GPGLL through USART interface,

1.In my schematics, my RF section is designed without Capacitors placed(open) , is capacitor need to be added, what capacitor value would you prefer .!2.Is we need to initialize and config for setting parameters in TESEO-LIV3F for GPRMC and GPGLL.Ple...

0693W00000APZArQAP.png
Snagu.11 by Associate II
  • 1189 Views
  • 1 replies
  • 0 kudos