Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32WB5MM Footprint

I'm looking to port a prototype from an STM32WB55 Nucleo board/custom daughter board combo to a single custom board using an STM32WB5MM module. I've done some digging but can't find a recommended footprint for this module. Does anybody know if one ...

RArch by Associate II
  • 664 Views
  • 0 replies
  • 0 kudos

BLUENRG stuck when writing BLUE_CTRL registers

I'm working on a custom board with a BLUENRG-2. I'm able to flash and erase with the UART and the SWD pins, but none of the programs work. When I debug it step by step, I find out that all programs hang on this line, when it writes on the BLUE_CTRL r...

0693W000008zoCVQAY.png
MRey.1 by Associate III
  • 713 Views
  • 2 replies
  • 0 kudos

Issue in STM32F746 - KSZ8863 interface

I'm trying to use a KSZ8863 Ethernet PHY with the STM32F746G. We have used the RMII interface to connect with KSZ8863 and running at 50MHz frequency .RMII pins are connected to KSZ8863 based on MAC mode interface.To test the KSZ8863 ,We have used stm...

STM-User by Associate II
  • 1076 Views
  • 0 replies
  • 0 kudos

Ble Receiving Junk data

hi all i am using blenrg2 m2sp chip as network mode. its operating as peripheral device and communicating with host controller through UART with 115200 baud rate .I received BLE read characteristic request , i did not response till 1 second ...

MCV.1 by Associate II
  • 2534 Views
  • 3 replies
  • 0 kudos