Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STSW-STUSB002 V1.11

Hello,I tried to upgrade STSW-STUSB002 V1.09 (early 2019) which works well with STUSB4500 chips, but doesn't with 4500L ones! Not same register mapping?..I installed STSW-STUSB002 V1.11 (early 2020) but no more "SINK PARAMETERS" on the GUI.Do I miss ...

MIMBE by Associate III
  • 1382 Views
  • 2 replies
  • 0 kudos

Range of BlueNRG-M2SA

Hello there,What's the total range of BlueNRG-M2SA? I read in this forum that is 33 meters, it's correct? My application needs something about 500 meters. Does possible reach it with BlueNRG-M2SA (or BlueNRG-2)?Best Regards,Leonardo

LTrin.1 by Associate II
  • 1034 Views
  • 1 replies
  • 0 kudos

Questions about Bluenrg-2N

Hello I'm in the development of the bluetooth communication between two bluenrg-2n devices. The bluenrg-2n are connected with stm32f405 through SPI. I'm not new in stm development but new in bluetooth communication. I've already done the init process...

Resolved! I2C1 ACK is not getting enabled in stm32f446re

I have configured the GPIO for I2C1(Alternate function 4) and enabled the Clock for I2C1. After that I am trying to enable the ACK. but not able to enable that.. Also tried for I2C2 and I2C3 facing the same issue.//enable the clock for the I2C periph...

PK by Associate II
  • 2851 Views
  • 6 replies
  • 0 kudos

Do I need more than one button on my device?

I have a simple project I am trying to implement using BLUENRG2-M2SA. It will connect with a user over BT and download a timer length. Then it will run the timer and blink lights when the timer counts to zero. The user then acknowledges the lights...

GGibb.1 by Associate II
  • 1672 Views
  • 2 replies
  • 0 kudos