User Activity

Hi All,There seems to be multiple bugs in the HCI implementation for WB series chips.Are there any newer builds of this image where these are fixed?Setup: Using reference dongle from P-NUCLEO-WB55.stm32wb5x_FUS_fw.bin latest version - 1.1.2stm32wb5x_...
Hello all,I have fond a fatal flaw in the 2.x BT library that comes with the latest SDK:STSW-BLUENRG1-DK 3.2.1Setup: bluenrg2, external balunProblem: When connecting a device using initial connection parameters with very small connection intervals (m...
Hello ST/Forum,I have a design where there seems to be confusion surrounding the inductor values and names:In the "PCB design guidelines" the inductors are name L14, L13 and L6.However, in the codebase, the inductors are called "RM1" and "PMU" induct...