STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Project structure using X-CUBE-USB-PD

Hello. I work on stm32CubeIDE. I am trying to figure out X-CUBE-USB-PD. An example of the project I'm trying to parse can be downloaded from the link https://github.com/STMicroelectronics/x-cube-usb-pd . It is required to understand how to adapt this...

DalOpez by Associate II
  • 263 Views
  • 0 replies
  • 0 kudos

Issues with PDM mono microphone with I2S

Dear all,I have some trouble setting up the correct acquisition of the MEMS microphone over I2S.Consider the STM32F401RE Nucleo board connected to the IMP34DT05 PDM microphone with L/R to GND.Through Mx, the I2S peripheral is configured as follows:Th...

0693W00000GYxgwQAD.png 0693W00000GYxe3QAD.png 0693W00000GYxi9QAD.png
frnt by Senior
  • 933 Views
  • 8 replies
  • 0 kudos

STM32F469I-DISCO CS43L22 Audio Codec

Hi! I am trying to generate a sine wave on my CS43L22 audio codec chip and use the included stereo jack on my STM32F469I-DISCO board. I'm using the STM32Cube IDE. There is one .WAV player example that I can't get to build in the IDE that's closely re...

Kneepatch by Associate III
  • 596 Views
  • 1 replies
  • 0 kudos

Play Audio files from Flash ic using cs43l22

Hi,i am using stm32f411e - Discovery Boardi want to know how to play any audio files through cs43l22i am using flash ic Doubt is that how to convert audio file into binary file save into flash memory & send the same to codec ic.only 2 audio files Kin...

Ss.61 by Associate III
  • 268 Views
  • 0 replies
  • 0 kudos

Speech input & output

Hi,I want to implement a speech IO using stm32f401 discovery board.In this case I am using the onboard digital microphone to acquire the PDM samples using spi2(I2S) interface. After that I am using the PDM filter to convert the PDM samples to PCM sam...

Configuring SAI to record mono on FS/LR low

I don't think that what I am asking is possible with the STM32476 that we are using, but it would be nice to have confirmation. We currently have a stereo setup that uses two I2S microphones hooked up to SAI1. Everything works great, but sometimes we...

jw56 by Associate III
  • 299 Views
  • 0 replies
  • 0 kudos