User Activity

I have got a custom PCB using STM32F4. I don't have any capacitor connected to the VCAP Pin and I wonder if this is necessary or not. Which is the use of VCAP and do I need to add it to my design? What can I do to solve my problem of no having one if...
I want to develop my own PCB using STM32F4. I want to use one external clock (16 MHz). I wonder where I have to connect the clock: OSCIN32-OSCOUT32 (pins 3 and 4) or OSCIN-OSCOUT (HSE) (pins 5 and 6 in STM32F446RET).I can see in the development board...
I want to interface two electret microphones (stereo sound) to STM32F446 chip. I don't know how to connect it or what protocol or pins I have to use. I have found a lot of information about digital microphones but nothing on this topic.Thanks.