STM32 Functional Safety
This follow up question of STM Functional Safety webinar. It was not clear from the webinar if drivers and device specific CMSIS code generated by STM32Cube is certified for functional safety standards?
This follow up question of STM Functional Safety webinar. It was not clear from the webinar if drivers and device specific CMSIS code generated by STM32Cube is certified for functional safety standards?
In my application, UCPD2 will be active for USB type C PD Sink (45W), which will be working together with other peripherals, such as timers, USB(DEVICE), etc. If the driving clock for UCPD2 is HSI16(in datasheet described), if no other choice, that m...
I'm trying to make a guitar pedal using the ADC on my F767ZI. I want to be able to perform an FFT and other functions on a buffer of data sampled at 48kHz.I wanted to use the ADC DMAs and use the equation Tconv = 12.5cycles + SampleTime, but I have n...
When I click on install or remove embedded software packages, using both install from local and use URL fail. When I have the package zip file local I get the error "The given file is not recognized as beeing (spelt wrong!) valid. It must either be a...
I want to test out the usb audio device middlweare but it seem the i can't recive any audio packet, the device is configured and stall after. no isochronous transfer is done. The code is just out from cubeMX with no modification. Is there more i have...
Hello,We have purchased the STM32F769I-DISCO KIT as we plan to use STM32F769I in USB audio IN/OUT application.I am trying to make "STM32CubeExpansion_USBAudioStreaming_V1.0.0" example provided by ST working. So far: I have configured the above exampl...
Hi,I'm trying to set up a simple test code for bi-directional audio streaming via USB using NUCLEO-H743ZI2 and a custom board with Cirrus CS4274 codec IC. I've tried and failed to find some documentation for CubeMX included USB Audio Class library (c...
This thread is a new problem discovered while investigating a different USB-PD issue in another thread. @Yohann M. recommended that I create a new thread for this issue. Here is the link to the other thread: https://community.st.com/s/feed/0D53W0000...
Why nothing work on first attempt???Howto solve this i need test USB UACEdit 1 I try too MX 5.4 same error zip file isnt pack WTF
Hi! i am using STM32F401CCU6 for BLDC/FOC motor control application.For foc application requirements, i need sampling 3 phase current in inject mode, vbus and motor temperature in regular mode.However, there is only 1 adc available for sampling. i tr...