2019-08-22 11:40 PM
When I click on install or remove embedded software packages, using both install from local and use URL fail. When I have the package zip file local I get the error "The given file is not recognized as beeing (spelt wrong!) valid. It must either be a MCU or CMIS pack". So I presume I do something else with this expansion pack as its not a MCU or a CMIS ?
2020-11-27 12:17 AM
Dear @mo'br ,
Could you please share the .ioc file and try to use the last available version of STM32CubeMX.
Kind regards,
Houssem
2020-12-27 6:39 PM
I have the same problem. I tried CubeMX version 6.1.1. I don't have an .ioc file because this happens before creating a project.
I'm also wondering why the Audio package does not appear in the list in the Embedded Software Packages Manager along with the other X-CUBE-* entries.
2021-08-01 5:40 PM
ST programming guru's answer