STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 USB audio difficulties

Hi there, I'm trying to make a basic USB audio speaker from an STM32H7 Nucleo board. I am fairly familiar with the USB audio middleware having studied it for a few days, but am not having much luck receiving audio data. I intend to use the built-in...

Mttjcksn by Associate III
  • 843 Views
  • 6 replies
  • 0 kudos

How to enable pdm2pcm middleware?

STM32F4-DISCOVERY board: I need to read from the mic (MP45DT02) and I was trying to use the STM32CubeIDE to generate the initialization and I cannot get to enable the pdm2pcm middleware. I have tried to configure I2S2 (no errors) but still pcm2pcm is...

RLecu by Associate II
  • 895 Views
  • 4 replies
  • 2 kudos

Resolved! Where are peripherals initialized?

I am implementing a USBPD application, using the NUCLEO-G474RE example of x-cube-usbpdm1 (it is called TCPP01_Consumer).The example works fine, but I am a bit confused as to where all the peripherals are initalized. The MX init functions are generate...

FGeig.1 by Associate III
  • 517 Views
  • 2 replies
  • 0 kudos

SAI - get best clock accuracy

Hi This is related to my other post (https://community.st.com/s/question/0D53W00000EcBvNSAV/sai-no-signal-on-mclk-pin) but I thought it would be more organised to make two posts since the question is different.How do I get the best audio clock accur...

0693W000002lgZ0QAI.png
SLasn.1 by Associate II
  • 1473 Views
  • 11 replies
  • 0 kudos

Resolved! STM32CubeMX & X-CUBE-USB-PD

Hello!I am trying to create my own USB PD device, but initially I want to test it using P-NUCLEO-USB002 kit. And I don't understand how correct install the X-CUBE-USB-PD library. I tryed to do it from CubeMX (V5.6.1), but there is no such extension i...

0693W000001qEb4QAE.png
Eremizin by Associate II
  • 497 Views
  • 3 replies
  • 0 kudos

I2S_CKIN Not Displaying in SAI UI

Hi there!When I set up a fresh project for the STM32G431KB in STM32CubeIDE, let's say I want the SAI to be clocked by an external clock source.So, in the prefs, I set Audio Clock Input (I2S_CKIN):Then I set up my Clock Configuration:Now one would exp...

0693W000001cc9aQAA.jpg 0693W000001ccA9QAI.jpg 0693W000001cc3yQAA.jpg 0693W000001ccBvQAI.jpg
etheory by Senior II
  • 330 Views
  • 1 replies
  • 0 kudos

Fresh install of CubeMX 5.6 - can't install latest CMSIS, CUBE-LRWAN, MEMSMIC, analog, timcooker libraries - all report .pdsc failure?

Trying to do a build of STM32L073, with latest CMSIS, LRWAN, MEMSMIC, and other libraries, but all seem to fail install into CubeMX on Win10. All install attempts report some .pdsc database failure. This is a new / clean install, and trying to add pa...

TZiel.1 by Associate II
  • 290 Views
  • 0 replies
  • 0 kudos