Hi all,we have a P-NUCLEO-USB002 kit, and there is a pre-programmed demo image on kitthe demo image will output CLI to operate, (please refer to the attached picture.)but there is not found in the STUSB010 library.could you share the information of w...
Hi,I would like to use the I2C2 (from I2C3) in "STM32G474_MB1303_DRP_ONLY"besides, modify I2C3_SDA to I2C2_SDA (pc9 to pa8), I2C3_SCL to I2C2_SCL(pc8 to pa9), the AF to GPIO_AF4_I2C2, ...
I have tried the application "STM32G474_MB1303_DRP_ONLY" from STUSB014-v1.1.1 to start my development. but there is a build break by some function in usbpd_core.h.But the related files and libraries are included in my project and listed in the projec...