Question
STM32F401 USB CDC stuck in IRQ loop
Posted on February 18, 2015 at 10:27
Hi,
I'm using the USB Host library 2.1.0 (with USB_OTG_FS) on an STM32F401CD. Using the USB CDC code I'm having the following issue:When the STM32 is connected to a PC but no application on the PC has the port open, the STM32 gets stuck in an interrupt loop:- USBD_OTG_ISR_Handler (at inepint handler)
- DCD_HandleInEP_ISR (at emptyintr handler)
- DCD_WriteEmptyTxFifo