Posted on December 04, 2017 at 09:10 Hello everybody, Since the release of the new documentation (Datasheet V5 and Command Guide V2), I'm looking for more detailed informations about SPI interface, SPI timing and SPI dialogue.... but the new doc ...
Posted on November 21, 2017 at 11:46 Hello, I know my question is simple but the answer, I think, is not as simple. Here is my use case: I would like to exchange a small amount of data between a PC (client) and a remote device (server) quickl...
Posted on November 14, 2017 at 18:30Hello,I am using the SPWF04 to provide Wifi acces to my system, interfacing by SPI. SPI works fine but I receive the following 'Console active' WIND message:02 10 00 02 00 0d syncKOE : WINDIndication Nb : WIND ID ...
Posted on October 04, 2017 at 11:31Since I have started to work with SPWF04SA, I have seen lots of mistakes in the documentation (specially about the SPI interface). Hopefully, the community help me but I wonder when the new version of the doc will ...
Posted on January 22, 2018 at 16:36For the people who would have an example of the SOCKDW command timing:1) SOCKDW command2) data payload3) AT-S.OKSPI run at 8MHz, nHost interrupt line is not shown but CS line can give you an idea of the interrupt r...
Posted on December 07, 2017 at 15:39 So, the upgrade goes well but does not solve the SOCKDW issue as you can see on the picture: I don't understand why I have an interrupt and 00s after I send my command and the payload. It cause bad behaviou...
Posted on December 05, 2017 at 11:33 Thank you, it gives me confidence to do the upgrade process. I will mark the subject as answered as soon as I upgrade and test it.
Posted on December 05, 2017 at 08:46Ok, your answer confirm what I record on my board.And it is really, really bad for my application because the Master can not wait that the module is ready to continue to work.It is mandatory that the Master can se...
Posted on December 04, 2017 at 19:14Yes, I use the FW1.0.0. Sorry, I didn't say it.Thanks for the informations, it is good to know.Could you tell me if the procedure (in the reply) in this post:https://community.st.com/0D50X00009XkXVJSA3 also applie...