User Activity

I'm using the BlueNRG-LP and want to enable "Readout Protection". From the reference manual RM0479 it can be enabled by writing the UserKey 0xAAAAAAAA to DATA0/1. In the RF-Flasher 4.3.5 Openocd readout_protection.cfg file writes the UserKey 0xFCBCEC...
Hi,I'm using a STLink-V3PWR. I have seen in the doc AN5999 that it's possible with the bridge to measure current/power consumption. Is there any DLL/API/Lib or C-Code example available for this?BR Sebastian
Hello,is it possible to enable/disable the "readout protection via SWD/JTAG mode for BlueNRG devices? Is it possible with openocd?BR Sebastian
Hello,I'm using BlueNRG-LP device and program my FW with RF-Flasher 4.3.0 in SWD mode. I set the "Readout Protection". Afterwards I cannot access the device anymore. From the manual RM0479 "Readout Protection" can be disabled with a mass erase. So I ...