Relating to STUSB4700 / 4710 datasheet I suggest the device address is the same as for 4700 with all adr pins set to 0.But no description in 4761 datasheet for I2C interface or register map.
Hi,we are using the STSW-STUSB006 I2C Lib whose only pupose is the programming of the STUSB4761 with an own MCU. What else does ST think what the Customers will do with it?The datasheet explicit describes multiple reprogramming and what to do that th...
@NBALL wrote:There is no register description for stusb4761 because this USBPD standalone controller is supposed to be used in AC adapter without any MCU.But some of your Customers want to use the STUSB4761 in an MCU application.We reconfigure the 47...
Situation on STUSB4716 is unpleasant.No register description available and without a doubt different to 4700A.You have to use STSW-STUSB005 tool to create and export a NVM configuration but you never know which bit does what.First PDO Profile is alwa...