STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bad parameters error for AES CBC encryption

I'm using cmox_ecdh for generating shared key for STM32G431KBT6. I tried using single call API from AES_CBC_EncryptDecrypt example and provided Computed_Secret instead of Key in cmox_cipher_encrypt function but I get bad parameters error. I dWith the...

mickey by Associate II
  • 1101 Views
  • 0 replies
  • 0 kudos

Resolved! How to create signed firmware for STM32U5 MCU?

Hi ST Team,I am using STM32U575 MCU. I want to create signed binary. I want to upload signed firmware in MCU and also update only new signed firmware via Native bootloader and want to restrict unknown firmware updates.How can I create signed firmware...

vijay_03 by Associate II
  • 4335 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U5 RDP regression without JTAG/SWD

Hello ST Community,There was a thread by Aurelien about this topic, but I did not understand the answer. So let me rephrase the question with my own words.I have a STM32U5 based device with high security settings (TZEN=1, RDP=2). Is there any other m...

ELuca.2 by Associate II
  • 2706 Views
  • 3 replies
  • 0 kudos

Resolved! Moving STM32U585 back from RDP level 2 to blank state

Hello,I need a quick confirmation. Assuming I have correctly provisioned OEM1KEY and OEM2KEY and I don't use OTP memory, I will always be able to revert my STM32U585 chip from RDP level 2 to blank state (RDP level 0, erased Flash, TrustZone disabled)...

ELuca.2 by Associate II
  • 2599 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F413H SBSFU

Hello,I am working on integrating SBSFU with the STM32F4 controller. The target controller is F429.I am trying to build an example project. It is a single image slot project which is developed for STM32F413H. I build the SE_Corebin project first and ...

ADani by Associate III
  • 2896 Views
  • 4 replies
  • 0 kudos