User Activity

STM32 Trusted Package Creator v2.12.0 creates incorrect option bytes which have 8 rows and no "reserved" last row As per AN5054, it should have exactly 9 rows The option bytes csv created from STPC v2.12 This leads to SFI programming failure. Am I mi...
The SBSFU framework allows users to employ multiple image signing keys, ECCKEY1, ECCKEY2, and ECCKEY3.Is there a method to blacklist ECCKEY1 and replace it with ECCKEY4, which may be transmitted via a key replacement update package if the private key...
Device details :ST-LINK SN : 002F003F3137510539383538ST-LINK FW : V3J9M3B5S1Board    : STLINK-V3SETVoltage   : 3.76VSWD freq  : 24000 KHzConnect mode: Hot PlugReset mode : Software resetDevice ID  : 0x480Revision ID : --Device name : STM32H7A/BFlash ...
Is there a an option to implement  SE_<FOO> in se_crypto_bootloader.c. I tried implementing a SE_FOO but the system reset as mentioned in document ."Protected code and data are accessible through a single entry point (call gate mechanism) and it is t...
Setup:Device - STM32H7B3I-DKProject - STM32H7B3I-DK\Applications\2_Images_ExtFlashWe have Composite firmware update file which contains and stored in external flash which Boot loader will process APP firmware (UserApp.sfb )GUI resources Calibration d...
Kudos from