STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Asymmetric Cryptography in STM

Hello,I’m working on a project using the STM32WLxx MCU and need guidance on implementing asymmetric cryptography (encryption, decryption, and key management). The MCU supports AES for symmetric encryption, but I’m looking for a solution for asymmetri...

Anubrata by Associate
  • 1494 Views
  • 1 replies
  • 2 kudos

Resolved! SBSFU STM32l476

Hi,I am working on SBSFU with stm32L476 Nucleo Board I am following the steps of Tutorial Security Part6 - STM32 security ecosystem - 02 Building the SBSFUI have Download Stm32CubeExpansion_SBFU_V2.6 but which is the highlighted directory are missing...

Prakash_Raj1994_1-1734591463772.png

Resolved! is RDP LEVEL 1  Enough?

hiplease only ST Employee answer this questioni use  this code for enable RDP LEVEL 1  for STM32H743 and STM32F407Can this code alone protect the program in the flash from any type of attack to read the program in the microcontroller?Will it be possi...

Natali by Associate III
  • 2529 Views
  • 3 replies
  • 3 kudos

Resolved! STM32H7B0VBT6 External Loader

I am using the STM32H7B0VBT6 microcontroller, which has limited internal flash memory. To implement Secure Boot and Secure Firmware Update (SBSFU), I have connected an external W25Q256JVIQ flash memory to the MCU via Quad SPI.   Is it possible to sto...

STM32L5 J-Flash RDP Level 2 using

Hello,I am trying to use below file to enable RDP 2 on an STM32 L552 controller.wiki.segger.com/images/7/78/STM32L5_Lock.jflash This has exit step "ExitStep21_Action" that set the DRP Level 1, However, I need to set RDP Level 2 by setting the value a...

Unprotect Flash to write a new Bootloader

I'm using a STM32F103RCT6Flash contains my own boot loader in pages 0 thru 10 and main application in 11 thru 61.When the device is flashed in manufacturing, protection is set to prevent reading and writing via the jtag port.I need to update the boot...

Joe.H by Senior
  • 1648 Views
  • 1 replies
  • 0 kudos

HAL_CRYPEx_AES() maximum number of output bytes?

I am using an STM32L4S9ZIJX part and attempting to encrypt a 256KB buffer (actually 262,144 - 16 = 262,128 bytes) using AES256 CTR mode in polling mode.I created a wrapper function to perform the encryption: int encrypt_CTR_mode(uint8_t* key, uint8_t...

dsorber by Associate II
  • 1374 Views
  • 2 replies
  • 0 kudos

SBSFU not detecting Active Slot Image

I'm working on integrating the latest SBSFU (v2.6.2) onto an STM32L4A6 platform. I've reviewed both the user manual and application note for the SBSFU, as well as the examples provided.In my use case:I have an external attached MMC flashI'm not plann...

jmcoreymv by Associate III
  • 6234 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.