STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 AES GCM Tag mismatch

Hi,I am trying to send encrypted data between a C# application and STM32 in AES GCM mode.Currently, I am only doing encryption of a known test vector.Key and IV are both all zeros.AAD length is 0.My testvector is: 00 00 00 00 00 01 00 00 00 00 00 00 ...

Dimlite by Associate III
  • 1167 Views
  • 3 replies
  • 1 kudos

STM32H573 code protection

How can the debug interface on the STM32H573 be permanently locked via nonvolatile configuration or fuse?The SBS chapter of the manual saysThe debug configuration can be locked thanks to DBGCFG_LOCK in SBS_DBGLOCKR.SBS_DBGCR is then no longer writabl...

abba by Associate II
  • 778 Views
  • 3 replies
  • 0 kudos

STSAFE-A120 Symmetric Decryption Support

Hello,We are working on an STM32F469/79-based device that uses SBSFU, which we are seeking to modify to use the STSAFE-A120 to perform the authentication and decryption algorithms.Section 2.7 of the STSAFE-A120 datasheet includes that the STSAFE-A120...

STSAFE-A120 Documentation

If, like me, you are attempting to use this device and believe there are gaps in the information available, you are correct. However, the information you seek, plus additional advice and assistance is available from ST, you simply have to ask via a t...

SHA-256 calculation of data on STM32L562 MCU

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code Hello, I need to calculate SHA-256 on STM32L56...

Does Stm32l496zgt6 have AES hardware

Hi,I'm working on STM32L496 for some security application, as per L4 series documents I see that L4 series controllers has AES hardware, but in my IOC settings under security option I don't see the AES. Why is this? does it mean STM32L496 doesn't hav...

ML2020 by Associate
  • 2685 Views
  • 4 replies
  • 2 kudos

Custom bootloader in SBSFU in STM32H753

Hi Team,  I am trying to add a Secondary/custom bootloader in SBSFU. But not able to figure it out how to do it. I changed memory for active slot area and used the same area for custom bootloader in both linker file of both SBSFU and custom bootloade...

How to integrate crypth AES-128 method in stm32f767

I'm currently working on a final project titled "Design and Communication Security Mechanisms in an Embedded Gateway Module for Electric Vehicle Networks." I'll be creating a security mechanism using AES-128 and a hash function, and securing data fro...

Adill by Associate
  • 473 Views
  • 0 replies
  • 0 kudos