STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Port fails on __IS_SFU_RESERVED()

Hi,I've been trying to port the STM32H753 SBSFU project to the STM32H735G-DK.The bootloader fails in SFU_BOOT_Init due to failing SE_Init().This is the result of __IS_SFU_RESERVED() failing it's test: 0x08008A00 < 0x08008061 < 0x0801FFFF (SB_REGION_R...

Arno1 by Senior
  • 1836 Views
  • 5 replies
  • 0 kudos

Resolved! How to use RNG on STM32H743ZI2?

I would like to use the RNG of the H743ZI2. The provided example works, but on a new project I can't get it work, The CPU clock is configured to 400MHz just like in the example./* RNG Initialization */   if (HAL_RNG_DeInit(&hrng) != HAL_OK) { /* ...

MLang.7 by Associate III
  • 4504 Views
  • 7 replies
  • 0 kudos

STM32L552CCT6 Read Protection Question

I want to apply Read Protection to the STM32L552CCT6 .​If you execute HAL_FLASH_OB_Launch(); after setting Read Protection, reboot does not work.​Read Protection is applied only when the power is physically rebooted.I want Read Protection to be appli...

KJoon.1 by Associate
  • 1221 Views
  • 2 replies
  • 0 kudos

Stack Heap Size of STM32G474VE

HiWhat is the maximum Stack and Heap size of a STM32G474VE with the SBSFU Bootloader 2 Image version?In the icf file the settings are at 0x400 and 0x200 which is really low./*-Sizes-*/ define symbol __ICFEDIT_size_cstack__ = 0x400; define symbol __IC...

dominik by Senior
  • 986 Views
  • 0 replies
  • 0 kudos

Can the STM32H723VGH6 implement an encrypted bootloader?

The STM32H733VGH6 datasheet specifically mentions "Bootloader with security services support (SFI and SB-SFU)," while the STM32H723VGH6 does not. Does that mean that I can't use encrypted firmware on the STM32H723VGH6?I tried to do some research, but...

Question on counter initial value for AES CTR on STM32WB

HelloIn chapter 22.4.9 of RM0434 Rev6 is stated:Counter: a 32-bit big-endian integer that is incremented each time a blockprocessing is completed. The initial value of the counter must be set to 1.Why can be the initial value of the counter not be se...

PADAM.1 by Associate III
  • 1590 Views
  • 1 replies
  • 0 kudos