STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using CHCHA20 crypto functions (STM32 CryptoLib 3.1.5)

Hello everyone,I was wondering the proper way to use the STM32_CHACHA_20_Encrypt() and STM32_CHACHA_20_Decrypt() functions available on the ST CryptoLib. I run the standard demo code on a STM32F072C8 MCU and it apparently run correctly, returning PAS...

GCalin by Associate II
  • 1055 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L476G-EVAL CRYP Examples Problem

The code from the 1.16 example builds fine in the EWARM. It writes the source blocks to the terminal, but as I see in the debugger, it fails to encrypt the input block. That times out as it fails to return a HAL_OK status. /* Start decrypting aCypher...

TZeig.1 by Associate II
  • 2665 Views
  • 5 replies
  • 0 kudos

NUCLEO-L152RE_2_Images_UserApp post build fails

I have the nucleo l152RE board and am trying to use this for following the mooc on sbsfu. It is possible for me to build (in cube IDE) both SECoreBin and SBSFU images. however, when building the UserApp it fails on the postbuild script. During build,...

STM32F read-out protection basically useless?

I know this was cracked before, but required high skills and expensive equipment, but nowthis method makes it really easy, basically anyone can do it.Any official statement concerning this from ST?Like the list of devices which are affected, possible...

Resolved! STM32H753AI SFI (Secure Firmware Install) questions?

Hello community,I have a few of questions regarding SFI:1) Does STM32H753AI support SFI (Secure Firmware Install)?2) Can I use SWD for the SFI?3) Is there any recommended HSM smart card reader for the SFI?Thank you :)

IFrid.1 by Associate
  • 1885 Views
  • 2 replies
  • 0 kudos

STM32H750 Hash peripheral issue

Hi all,I have two different batches of Revision V STM32H750VBT6. All units in one of the batches (Date Code 045) has issue with the hash peripheral while the one (Date Code 928) is working completely fine.I created a new basic project for testing thi...

0693W000007ZMTUQA4.png 0693W000007ZMWMQA4.png
CShen by Associate
  • 2065 Views
  • 3 replies
  • 0 kudos

Resolved! Does SBSFU support user app to execute from both Bank 1 and Bank 2?

I am using STM32L4A6VG with 1 MB flash and my application is about 600+KB. I want to update the user app from an external flash and need some guide to modify SBSFU.​After reading these 2 examples (STM32CubeExpansion_SBSFU_V2.4.0\Projects\B-L475E-IOT0...

SL61 by Associate II
  • 3697 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.