STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I use STM32G0B1 with SBSFU 2_Images?

Hi,I find the new chip STM32G0B1 from STM32CubeMX.And I want use this chip with SBSFU 2_Images.But I can not find the STM32G0B1 project from the X-CUBE-SBSFU v2.4.0.Is STM32G0B1 compatible with X-CUBE-SBSFU v2.4.0 ?How do I use STM32G0B1 with SBSFU 2...

EEdwa.1 by Associate III
  • 1066 Views
  • 1 replies
  • 0 kudos

Can't close Lab projects - File access rights

During the workshop itself, I had some problems with some of the example files not having correct access rights to allow the workshop changes to be made.We worked around that during the workshop.Now I have just come back to the STM32Cube IDE; it star...

0693W000006HauSQAS.png 0693W000006HauwQAC.png 0693W000006Hb0kQAC.png 0693W000006Hb2WQAS.png

Resolved! STM32H75x - How to erase properly with removal of secure area?

I have some code that removes a "secure area" on STM32H75x by so called "regression" from RDP level 1 to level 0, which causes full erase.(Actually this code is based on example very kindly provided by ST support) void EraseAll(void) { uint32_t fla...

Pavel A. by Super User
  • 2278 Views
  • 4 replies
  • 0 kudos

Resolved! Unable to find definition of FW_INFO_TOT_LEN

I'm trying to port the SBSFU to STM32H735. I started from the project for the NUCLEO-H753ZI.I get errors in sfu_fwimg_core.c on FW_INFO_TOT_LEN but where is this defined?A simple grep -r turns up nothing.Thanks!

Arno1 by Senior
  • 1938 Views
  • 6 replies
  • 0 kudos

Endianness of 'in the air' data bytes on STM32WLE5 - I asked this question before but did not get a definitive answer. So hoping someone here can answer now. I can get no response from STM online support. HOW DOES ONE GET AN ANSWER FROM STM ??

We are evaluating if we can use the STM32WLE5, to interface to existing devices .A critical factor is the expected endianness of the data. I have seen no reference in the docs if this can be set, so I have provided an example message and would like t...

JNoci.1 by Associate II
  • 5289 Views
  • 6 replies
  • 0 kudos

Usage of STM32 crypto library (UM1924) on STM32WB

Hello,one question (or feature request):I try to use the STM32 crypto library (v1.3.1 software implementation) on STM32WB. I activated the RNG and CRC but the calculated results (encryption/decryption, cmac) are not ok. Are there other things to do?I...

PADAM.1 by Associate III
  • 1789 Views
  • 3 replies
  • 0 kudos

How can I calculate CRC of image in post build?

Hello,I want to calculate the CRC (32 bit) of image at post build and insert it in a known location in the image.In order to do it I should perform the following steps:a) Definition of placeholder in linker script fileb) Post build steps: b.1) Ca...

YHass.14 by Senior
  • 13332 Views
  • 16 replies
  • 0 kudos