STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HardFault when transfer control from BL to APP

Hi,Device - STM32H7B3I-DKProject - STM32H7B3I-DK\Applications\2_Images_ExtFlashHardFault when transfer control from BL to APP1) Last trace of codelaunch_application: /****************************************************** * return from exception to a...

0693W00000HqonPQAR.png 0693W00000HqonyQAB.png 0693W00000HqopGQAR.png
Grogu by Associate III
  • 1393 Views
  • 1 replies
  • 0 kudos

SBSFU - STM32H755 Optimization Problem

I'm working on a project with SBSFU implemented on STM32H755. I'm using slot 1 for CM7 and slot 2 for CM4. I'm using the IAR workbench. Both CM4 and CM7 hex files work just fine in debug mode and everything seems to work with SBSFU implementation. Bu...

YChen.16 by Associate
  • 1444 Views
  • 1 replies
  • 0 kudos

Hash using without hash processor

I'm learning using cryptography method on stm32f429. But there is no Hash proccesor on the system. Although there is no hash proccessor, could I use the STM32CubeCrypto Libraries HASH examples on my board ? What kind of changes if my proccessor ha...

DCtech by Associate II
  • 1165 Views
  • 2 replies
  • 0 kudos

Getting the HAL_CRC module to generate a CRC32

I'm trying to get the HAL_CRC module to generate a 32bit CRC32 that matches the online calculators and matches what I get out of python with binascii.crc32() or zlib. I have a DoCkecksum() call below that calls HAL_CRC_Calculate() and I have called ...

ttatakis by Associate III
  • 2569 Views
  • 2 replies
  • 0 kudos

St Crypto library upgrade issue V2.0.6 -> V4.0.1

We had a project built using ST Crypto V2.0.6 (M3_CryptoHW_2_0_6.lib) library in Keil IDE. Now we replaced the ST Crypto library by V4.0.1 (libSTM32Cryptographic_CM3.a)We are seeing the following errors..\STM32_Crypto\lib\libSTM32Cryptographic_CM3.a(...

0693W00000HppBoQAJ.png

SBSFU - Start in different flash memory sector

Hi,I'm using a STM32F722RE and in my current application, I used sector 2 and 3 of the flash as a virtual EEPROM. The memory of the controller looks like this: So sector 4 should be enough for the SBSFU and I would like to set my application to secto...

0693W00000Hq5mlQAB.png
STsch.1 by Associate III
  • 4058 Views
  • 8 replies
  • 1 kudos

Hi I am new to SBSFU I had run the SBSFU example for STM32G474 after execution I have receive the welcome window along with menu option but I am unable to chose the option after pressing key it cannot take that input what should I do? pls help me

According to me there is problem in Receive call back function but I don't understand what should I do to resolve this....Please find the attached screenshot for understanding.In that screenshot we are able to see 1 to 5 option but after pressing 1 o...

p123 by Associate II
  • 1710 Views
  • 2 replies
  • 0 kudos

How can I port the SBSFU to another board?

Hi,I'm using a STM32F446RE Discovery board and would like to test the SBSFU on it. At them moment, I take the example code from the STM32F413H Discovery board, but I'm not sure what I'm doing wrong to never get access over the tera terminal. What I h...

0693W00000HpvhlQAB.png 0693W00000HpvieQAB.png 0693W00000HpvsAQAR.png
STsch.1 by Associate III
  • 1595 Views
  • 1 replies
  • 1 kudos

SBSFU Flash overflow

Hi,I have some trouble with using the SBSFU. In the first place, I could not build the SECoreBin project, but I found out, it was the path length in Windows making me the trouble. Now, after solving this and building a complete new project example, I...

0693W00000HpwfTQAR.png
STsch.1 by Associate III
  • 909 Views
  • 2 replies
  • 0 kudos