User Activity

Hi,I find the new chip STM32G0B1 from STM32CubeMX.And I want use this chip with SBSFU 2_Images.But I can not find the STM32G0B1 project from the X-CUBE-SBSFU v2.4.0.Is STM32G0B1 compatible with X-CUBE-SBSFU v2.4.0 ?How do I use STM32G0B1 with SBSFU 2...
Hi,I have download the newest version SBSFU v2.4.0.From the readme.txt, I compile the SBSFU project NUCLEO-G071RB 1_Image_SBSFU with the MINICOM_YMODEM switch enabled (app_sfu.h).But send the user encrypted firmware file UserApp.sfb always failed.How...
Hi,According to the document "AN5056-Integration guide for the X-CUBE-SBSFUSTM32Cube Expansion Package" Table 3. SBSFU code size reduction,In project "NUCLEO-G071RB", I build "1_Image_SECoreBin" by modify SECBOOT_CRYPTO_SCHEME from "SECBOOT_ECCDSA_WI...
I build Projects "NUCLEO-G071RB" in X-CUBE-SBSFU and load "SBSFU.bin" into the board.After reset the board, I download firmware "UserApp.sfb" with SecureCRT by using menu "Transfer > Send Ymodem" , but it failed.I also try to use "Tera Term", it dow...