STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TFM_Loader_NonSecure problem.

Dear Sir.I am using the example TFM_Loade_Non_Secure , It compiles I set for Download NonSecure App Image , when I send any file*.elf with TeraTerm.File,Transfer.YMODEM.Send , then the programreply with "Abortes by user".Please Advise

How to properly configure STM32U585 to use DMA in secure mode (TZEN = 1) to send data from internal Flash (non secure zone) to Hash (in secure mode)?

Hi,I want to know a properly way do to that.If i use standard configuration I run hard fault as soon as DMA start (linklist mode) (HAL_HASHEx_SHA256_Start_DMA).I put Fault Analyser details Source/Destination secure bit are set before calling this fu...

0693W00000YAa7YQAT.png
Aurelien1 by Associate III
  • 2103 Views
  • 2 replies
  • 0 kudos

SPI with DMA and CRC : data corrupted by DMA ?

I'm running SPI with DMA and CRC enable between two stm32, slave is stm32f415 MCU.Sometimes it appears that data received is corrupted whereas CRC check gives no error. For instance (polynomial used is 0x1021)Normal behavior:3 words sent: 0xAAA0; 0x0...

JJim.1 by Associate
  • 1212 Views
  • 0 replies
  • 0 kudos

STM32H745 replacement issue

I use STM32H755ZI to configure the product, but the market is out of stock, can I use STM32H745/STM32H757/STM32H747 instead?Assuming I'm not using CryptoHash/SFI/SBSFU and MIPI-DSIIs LQFP144 pin to pin?

Resolved! STM32G0B0CE PIN 2 PIN mcu chip replacement selection

We would need to implement Secureboot & secure FW upgrade feature in one project.I find both STM32G0B0CE and STM32G0B1RET6 not support RNG.But the blow link shows they both support SecurebootX-CUBE-SBSFU - Secure boot & secure firmware update softwar...

Carlos.K by Associate II
  • 2549 Views
  • 4 replies
  • 1 kudos

Resolved! Design flaw in HAL?

I am using CubeIDE 1.11.2 with a STM32F3DISCOVERY board and have created an IDE project via the integrated CubeMX GUI.I want to activate read protection via HAL_FLASHEx_OBProgram as well as the write protection for the FLASH area of my firmware (appl...