STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Has anyone managed to get the STM32 hardware CRC on STM32F7XX to match the output of srec_cat.exe when using the -STM32_Little_Endian flag?

srec_cat.exe has a flag -STM32_Little_Endian described in the srec_cat manual as "These filters many be use to generate the CRC used by the hardware CRC unit on the STM32 series of ARM MPUs.". I can successfully append a CRC to my firmware file using...

HMcKi by Associate III
  • 2231 Views
  • 2 replies
  • 0 kudos

STM32H7 Flash-embedded CRC HW calculation

We are using a STM32H7 microcontroller for our project ans would like to use the HW CRC embedded in the Flash module.We are designing a custom bootloader that will calculate the CRC and then write it in a reserved section of the flash. Since the devi...

CRC32 questions

Hi,I have a general question regarding CRC32 for data read from flash. For example I am reading 2048 bytes of data total 512 bytes chunk each time. My question isdoes it make any difference if I check CRC32 for every 512 bytes read or after read of 2...

readout protection cracked on STM32

Posted on January 08, 2018 at 10:21 Am I correct that readout protection has a major issue and is not working at all? Are all STM32s affected? Any comments on this from ST? See here: https://www.aisec.fraunhofer.de/en/FirmwareProtection.html ...

AES 256 GCM Decryption on STM32L562

Hello,I am trying to decrypt some data on the L5. The data below can be fed directly into a python crypto library and get a valid result. I am trying to understand the 32-bit alignment requirements of the L5 as well as any possible byte swapping ne...

For a new line of products, we are considering STM32F750 but it lacks on-the-fly decryption support. Is there a new line of microcontrollers planned that matches the spec of STM32F750 but includes support for on-the-fly decryption

We need a powerful M7 core running at high speed + GPU support for TouchGFX. It seems that STM32F750 is a perfect match, apart from the fact that it is missing support for on-the-fly decryption (OTFD). As we would like to use external flash memory an...

tomptz by Associate II
  • 837 Views
  • 0 replies
  • 0 kudos

SBSFU User Application integration

HiI'm working on a ST STM32G474RE with the 2 Images and have a application with STM32CubeMX.I was reading the AN5056 but don't understand how I can build my application bin file to download with the Y-modem protocol. Or do I need to modify and add al...

dominik by Senior
  • 1899 Views
  • 4 replies
  • 0 kudos

include Crypto Library in STM32CubeIDE

hello,This is an old thread but I hope to get an answer here.I'm using NUCLEO-L496ZG-P, and I have data to decrypt (AES128 CBC).I'm using the STM32CubeIDE to compile.I'm trying to use the Cryptolib but didnt get how to do so. I did download "en.x-cu...

YLAZREG by Associate
  • 872 Views
  • 0 replies
  • 1 kudos