STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How can I display debug message in interrupt routine?

Hello,​I use stm32l412b / FreeRTOS.I use below function to display dubug message.The MCU is halted and a watchdog reset occurs when the function below is called in interrupt routie.​It works normally if not in interrupt Would you let me know what is...

MKim.12 by Associate II
  • 3176 Views
  • 6 replies
  • 0 kudos

FATFs with w25qxx problem

Hey,I have a problem with reading files larger than size of one sector of FATFs (4096 bytes).Reading seems to be done correctly until it reaches 4096th byte of file, then data is corrupted. The problem appears when one part of readen data is on one s...

KWier.2 by Associate II
  • 3456 Views
  • 7 replies
  • 0 kudos

STM32L552ZE-Q: SAI - I2S, problem on FS signal

Hi, I'm using SAI in I2S mode to play stereo wav file. Audio Data is sent to TAS5722l which is a Mono Audio amplifier. My problem is that the FS (Frame Synchronization) signal stays always at level High. This results in a stereo audio file being play...

Android app recognition device using USB CDC

hello.The product was developed using STM32L412RB / FREERTOS by two companies.There are apps from two companies using USB CDC.Their PID/VID is the same.Apps from two companies are installed on one phone.Phone is asking which app to use when my devic...

MKim.12 by Associate II
  • 874 Views
  • 0 replies
  • 0 kudos

Using USB-PD and USB-CDC together

Hello, I'm working on STM32G0B1KET6N uc with custom board.When I'm using this tutorial: https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink everything is working great, my device is acting as USB PD Sink. Bu...

Tarru by Associate II
  • 2374 Views
  • 2 replies
  • 0 kudos

Dual port ethernet switch interfacing in STM32H743

Hi Team,We are using STM32H743 microcontroller (as a server) interfaced with LAN9353/KSZ8863 with two ethernet ports, one port connected to PC (as 1st client) and another port connected to embedded board(as 2nd client). Till now we are able to check ...

PNaph.2 by Associate II
  • 3401 Views
  • 2 replies
  • 1 kudos

Problem with SMBus communication

Hi, I've been trying for a few days to communicate with a device by SMBus.The device is an Microchip USB2422 and for test I use board DISC1 with STM32F429 on i2c3 port.The problem is that when I try to communicate with it to oscilloscope I see only a...

SDall.11 by Associate III
  • 981 Views
  • 0 replies
  • 0 kudos