STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EPR Support for TCPP

Hello, I saw the thread below and now a bit confusedhttps://community.st.com/t5/stm32-mcus-embedded-software/update-about-usb-pd-stack-to-support-epr-mode/td-p/829168It says EPR is supported with a TCPP package but the TCPP-M18 itself - rated to 100W...

grisom13 by Associate III
  • 282 Views
  • 1 replies
  • 0 kudos

stm32f446re SAI with DMA transfer

I'm trying to make audio equipment using stm32f446re board and pcm5102 module. When I used the audio equipment, when I sent music using i2s communication, the output came out well, but when I finished DMA setting after selecting i2s protocol in sai, ...

화면 캡처 2026-02-20 232429.png 스크린샷 2026-02-20 232458.png

A submodule project in another project

Hello,I am working with STM32 IDE v2 and stm32u585 processors. I have a project which is configured with the help of stm32 cube mx and has its own core/Drivers/.ioc files. It is like a ground for using the processor together with other external modul...

GTanova by Associate III
  • 169 Views
  • 1 replies
  • 0 kudos

FDCAN / Zephyr issue

Custom board. STM32U5G9. I am running Zephyr and trying to use PB8 and PB9 for the FDCAN peripheral. In loopback mode, it does not get any errors but in normal mode it does. The odd thing is that if I change the pins in the dts file to PA11 and PA12,...

zeek-atc by Associate
  • 239 Views
  • 3 replies
  • 0 kudos