STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32WB55 USB Dongle MTD Not Receive CoAP Message

Hi,I'm using a STM32WB55RG Nucleo and STM32WB55 USB Dongle. I programmed the nucleo as FTD and write 2 sources and programmed the usb as MTD and write 2 sources that exactly the same with FTD. I'm trying to send coap messages from FTD to MTD so this ...

Resolved! STM32F103RCT6TR-CAN

Hi,          I am MURALI SELVAM I need one solution for STM32F103RCT6TR. Which is CAN pins in STM32F103RCT6TR IC. Kindly tell me. Thank you.

murali by Associate III
  • 2932 Views
  • 4 replies
  • 1 kudos

Resolved! 3 SPI busses does not parallelize data access

STM32H743We have 4 SPI busses running at 12.5MHz but the SPI clocks are sequentially. SPI 1 and 2 are using DMA Channel 1 while SPI 3 and 4 are using DMA Channel 2. We would like them to run in parallel.Can they run in parallel.The code uses HAL_SPI_...

rlegault_0-1705436036380.png
rlegault by Associate II
  • 1102 Views
  • 1 replies
  • 0 kudos