STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't enable port B & D clocks

I tried the following code in a STM32F107:RCC->AHBENR = RCC->AHBENR | RCC_APB2ENR_IOPBEN_Msk| RCC_APB2ENR_IOPDEN_Msk;and RCC->AHBENR = RCC->AHBENR | 0x00000008 | 0x00000020;When I display RCC->AHBENR, it always shows 0001C014.I expected to see 0x0001...

vneff by Associate III
  • 2816 Views
  • 5 replies
  • 2 kudos

Resolved! SPI Slave Receive Interrupt

I am trying to make a very simple SPI ISR to read the RXDR and store the value to a buffer. However, I cannot get the ISR to even trigger without using HAL_SPI_Receive_IT(). I do not want to use the callbacks or the default IRQ generated by cube. I c...

How to use HAL_GetTick ?

Dear Members,How can I use HAL_GetTick for time stamp ?Is this right ?or I need something else ?Thankscase PULSE_TRACE_UP: if(sensor_value > prev_sensor_value) { printf("PULSE TRACE_UP\r\n"); currentBeat = HAL_GetTick(); ...

Resolved! Issue in CAN Normal mode with STM32F412

If anyone Work on project that interfacing Can transceiver TJA1050 with STM32F412RET6 , if yes i hope  anyone send Example code that work and clock configurations ,, the loopback mode work correctly .. but in normal mode problems start ... and operat...

Resolved! STM32H7B0 ADC watchdog cannot stop interrupt

Dear,We using an ADC in our application at 1MspsThe ADC is always running in a circular DMA mode.To start the buffering of the samples we use the Analog watchdog 1. So when the input signal goes outside the analog watchdog thresholds the function "HA...

OGhis by Senior
  • 1641 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.