STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

data sharing between the cores

Hi,I'm using STM32H7 dual core, where the data has to be shared between the cores, so im having totally 21 variables totally 76 bytes, thought of do it like a structure, so where to place the structure exactly for this data sharing. so, this structur...

Cube/USB/CDC / bulk endpoints overlap?

Hi!EDIT: WARNING! This is no real fix... The bug remains...With STM32Cube_FW_F2_V1.9.0 and CDC's /dev/ttyACM0 I had funny glitches on VoidLinux, when i tried full duplex communication (host<>device):some packets never arrived at the USB hostsome shor...

RRIDDICC by Associate III
  • 217 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H747IIT6 ETHERNET RMII PROBLEM

Hello,I am using the STM32H747IIT6 microcontroller along with the LAN8742A Ethernet PHY, configured in RMII mode. However, I am facing issues where the Ethernet interface is not working at all in my circuit. It appears there may be multiple bugs or c...

KAnahar by Associate III
  • 1496 Views
  • 6 replies
  • 1 kudos

PDM2PCM(HP) library details

Good morning, if possible, I would like more details about the following PDM2PCM(HP version) library used for converting PDM data to PCM.           typedef struct{ uint16_t bit_order// MSB / LSB uint16_t endianness;// big endian / little endian uint3...

Mavi by Associate II
  • 1329 Views
  • 1 replies
  • 1 kudos

STM32H562 RTC problems

Hello everyone. How are you?I created a test program based on https://community.st.com/t5/stm32-mcus/how-to-calibrate-the-stm32-s-real-time-clock-rtc/ta-p/744958 I calibrated and compared the signal (512Hz @ PB2) with an oscilloscope, resulting in an...

Leandro_Araujo_0-1765540271056.png

LAN8720 With NUCLEO H723ZG

Hello everyone, I have a NUCLEO-H723ZG board and I would like to establish Ethernet communication with it. The board already includes a LAN8742 chip as the physical layer. However, in my system there is an external LAN8720 magnetic Ethernet module. A...