STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBC PD multiport TCPM/TCPC

Hi, We are developing PD multiport design with TCPM/TCPC architecture, but we've come across a post of CPM stack should be no longer supported for newer products. https://community.st.com/t5/stm32-mcus-embedded-software/usbc-pd-tcpm-on-the-stm32u5/m-...

petertan by Associate
  • 1250 Views
  • 3 replies
  • 0 kudos

H747 DSI use one data lane issue

First, let's introduce the usage environment.The Board is STM32H747I-DISCO, the LCD board is MB1166-A09,and the pack is STM32Cube_FW_H7_V1.11.0.Now I'll describe my issue. In the official routine LCD_DSI_CmdMode_SingleBuffer, DSI uses two data lanes ...

SONGTAOSI_0-1739430503878.png SONGTAOSI_1-1739431560522.png
SONGTAOSI by Associate II
  • 2542 Views
  • 3 replies
  • 1 kudos

Resolved! Paho MQTT : connexion aborted by STM32

Hello,I'm trying to implement the lwip + paho mqtt (embedded version) on a nucleo-f207zg board, following this project : https://blog.naver.com/eziya76/221938551688 I have a mosquitto broker and wireshark on a windows computer.Mosquitto started with ...

mosquitto.png wireshark.png
tarzan2 by Senior
  • 1824 Views
  • 1 replies
  • 0 kudos

Installing X-Cube-Audio in cubeIDE?

Hi all,I tried to install X-Cube-Audio in cubeIDE but it is not in the list of software packages. I tried to use "From local..." and pointed to the zip file but I got an error (picture below). There is an X-Cube-Audio-F7 that is obsolete but nothing ...

_legacyfs_online_stmicro_images_0693W00000dDYNLQA4.png
Rodo by Senior
  • 2471 Views
  • 2 replies
  • 0 kudos

WAV/MP3 player with STM32746G-Discovery.

Hello, I downloaded STM32CubeExpansion_Audio_V1.1.1 and I tested the MP3 player project (Audio_MP3_player) with an STM32746G-Discovery.It works very well.But now, I would like to add 2 or 3 additional functions but I have big gaps in development.I wo...

DB..1 by Associate II
  • 5316 Views
  • 7 replies
  • 0 kudos

FreeRTOS and lwip

Hi everyone!I'm sorry I just started with STM universe...Since twodays I try to start the lwip through freertos on my NUCLEO-H723ZG. For starting I generate the code with the CubeMX and try to call the MX_LWIP_Init() in a startAppTask. But ethernet_i...

Joe26 by Associate II
  • 2685 Views
  • 2 replies
  • 0 kudos

MDC / MDIO Read Write Failure

Hi All              I designed the hardware using the STM32H753VIT6 and the 3-port Ethernet switch KSZ9893RNXI. The STM32 is configured and can communicate with the external world via Ethernet. However, I'm unable to read or write to the switch regis...