STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

memcpy() function not working

Hi,I'm using the STM Cube IDE version 1.15.1 along with NucleoG474RE board. My C application requires the use of memcpy(). The memcpy() function should copy the values from an unsigned char source buffer to the unsigned char destination buffer. This ...

i2c error

Dear ST I have some question about i2c read functions Currently we use zephyr os (version 3.4.0) the stm32f412RGT used as the host and the host  reads a 5-byte value from another mcu used as a slave throughi2c the following problem occurs once every ...

hongjo_0-1742212846669.png
hongjo by Associate II
  • 2450 Views
  • 6 replies
  • 3 kudos

Stack overflow in freeartos and ethernet

HiI am using the evaluation board stm32743And testing the firmware that include freeartos and ethernetIf enabled the "check_for_stack_overflow" in cubeMx freeartos this will resultin vApplicationStackOverflowhook to inhabit.checking sp register when ...

dorong by Associate II
  • 2422 Views
  • 6 replies
  • 2 kudos

STM32 Audio Capture

Im using the B-U585I-IOT2A board. I want to have continuous audio capture and preprocess the audio into melspectrograms for input into a sound detection model. Im having trouble setting up the microphone. Is it the MDF1 setting in the peripherals? Im...

jzzunn by Associate II
  • 1081 Views
  • 1 replies
  • 1 kudos

STM32F7: Ethernet deadlock on TxCpltCallback

Hi, I have a problem with the Ethernet on a STM32F777 with CMSIS V2 and LWIP. Firmware package is 1.17.2. The configuration was created with CubeMX. The firmware runs normally until a data packet (ping command from cmd) is received on the Ethernet. T...

Sandro_K by Associate III
  • 4930 Views
  • 8 replies
  • 0 kudos