Skip to main content
Jungle
Associate
March 1, 2019
Solved

Bug in HAL_SetTickFreq function (F4 v1.23.0, 1.24.0)

  • March 1, 2019
  • 3 replies
  • 1545 views

I've already contacted support, so this post is just for community.

There's a bug in HAL_SetTickFreq function (stm32f4xx_hal.c)

---8<---

HAL_StatusTypeDef HAL_SetTickFreq(HAL_TickFreqTypeDef Freq)

{

 HAL_StatusTypeDef status = HAL_OK;

 assert_param(IS_TICKFREQ(Freq));

 if (uwTickFreq != Freq)

 {

  uwTickFreq = Freq;

  /* Apply the new tick Freq */

  status = HAL_InitTick(uwTickPrio);

 }

 return status;

}

--->8---

If HAL_InitTick fails, the frequency remains unchanged whereas uwTickFreq is changed. E.g. I have stm32f407vgt6 working on 168MHz with 1kHz SysTick . I want to set SysTick to 10Hz, so I call HAL_SetTickFreq( HAL_TICK_FREQ_10HZ ). Eventually SysTick_Config fails because (16800000 - 1) is bigger than SysTick_LOAD_RELOAD_Msk (0xFFFFFFUL). But uwTickFreq is already == HAL_TICK_FREQ_10HZ, so the ticks are now counted incorrectly. HAL_SetTickFreq function should be changed to something like this:

---8

...

 if (uwTickFreq != Freq)

 {

  /* Apply the new tick Freq */

  status = HAL_InitTick(uwTickPrio);

  if (HAL_OK == status) {

   uwTickFreq = Freq;

  }

 }

...

--->8---

This topic has been closed for replies.
Best answer by Imen.D

Hello @Jungle​ ,

We confirm this issue and passed it along to our development team for fix.

Thanks for your contribution.

Kind Regards,

Imen

3 replies

ST Technical Moderator
March 4, 2019

Hello @Jungle​ ,

Thanks for highlighting this issue.

We will check it internally, then we will come back to you with update.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
March 27, 2019

Hello @Jungle​ ,

We confirm this issue and passed it along to our development team for fix.

Thanks for your contribution.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Remi.G
Associate II
March 18, 2025

It appears that the implementation has picked up the proposed fix (I am using U5A5, CubeMX 6.14.0, pack v1.7.0), but that implementation is incorrect.

HAL_InitTick() uses the value of uwTickFreq. Since the "fix" only sets that after the call, the tick frequency never changes.

The correct fix would set uwTickFreq before the call, and restore it if the call fails. Better yet, add frequency as a parameter to HAL_InitTick(), or add a HAL_ChangeTick().