STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LTDC Display Type Restriction

I am using the STM32H743VIT and trying to integrate using LTDC. The Display Type options in CUBEMX only allow 16 or 18 bit RGB. I know there is no LTDC_R0, so I assume that is why there is not option for 24 bit RGB; however, we were just planning on ...

16384 points of FFT(Fast Fourier Transform)

Hello community, In my project requires upto 16384 points of FFT(Fast Fourier Transform) . I found out that I can’t perform this number of FFT points using arm CMSIS DSP library since it is limited to 4096 point Max. Due to this I have to use externa...

SA  V.1 by Senior
  • 7496 Views
  • 15 replies
  • 6 kudos

Resolved! Timer to DMA to SPI STM32H723 using LL

Hi,I want a GPIO pin to trigger an SPI transfer. The way that I have figured this should work is:PG3 -> TIM23 -> DMA2 -> SPI1 Here is basically what I have so far:/* Includes ---------------------------------------------------------------------------...

ZacJFrank by Associate II
  • 2028 Views
  • 5 replies
  • 0 kudos

Azure IOT STM32H735G-DK implememtation

Hi currently i am using  STM32H735G-DK  i need to implement Azure IOT using ThreadX 1. From CubeMX i have generated Drivers for MQTT,DNS,Cloud,DHCP,mdns,sntp in the cloud files where i can update my connection strings of my cloud Configured  Asset I ...

avinpat_8_0-1743679250297.png
avinpat_8 by Associate III
  • 1037 Views
  • 1 replies
  • 0 kudos

STM32L412 flash section writing isn't permanent

It has worked at times but at others is becoming all 0xFFFF or whatever values become written into unused areas.Currently it loses memory every time.My code reads a block of settings and looks at one location to check if it's zero, which indicates no...

CGadg by Associate III
  • 2916 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 Uart Overrun

Hello every one .this is my first post so excuse me if i do something wrong.I try to establish Uart Asynchronous line between two stm32f303k8 .one of them use basic timer to send 8 byte uint buffer every 200 mili-sec and the other use HAL_UART_Receiv...

yairyamin by Associate II
  • 13784 Views
  • 12 replies
  • 7 kudos

Resolved! Build doxygen

Hi,when building the Doxygen documentation locally, numerous warnings appear. Especially, errors like this:stm32g4xx_hal_driver/Inc/stm32g4xx_ll_lptim.h:605: warning: Found unknown command '@rmtoll' stm32g4xx_hal_driver/Inc/stm32g4xx_ll_lptim.h:601: ...

T B by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos