STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Virtual ComPort Example

Posted on October 03, 2011 at 20:38Hello, I have been searching without success to find an example of the STM32 Virtual Comport that shows how to receive data from the PC. I am coming from an 8051 background so the use of the legacy COM port will he...

flashing stm32-h107

Posted on September 17, 2011 at 14:10Hello I am a little confused about how to flash the code on to the target olimex stm32-h107 board. The board has the USB interface , so if it is possible to flash directly through usb , then please tell me how t...

stm32f2xx Bootloader

Posted on July 22, 2011 at 15:17Will there be a version of the Flash Loader Demo and the DfuSe Demo available for the STM32F2 series?   I've tried to get both of these to work with a STM3220G Eval board but they don't seem to be compatible, or am I ...

Boot loop issue.

Posted on September 12, 2011 at 17:58Hi there, I'm new to STM32 and I've been working with STM32 Discovery kit without any serious problems. Now, I designed my own demoboard with STM32F103RCT6. I'm using Atollic Truestudio Lite and Discovery kit as ...

USB Product ID Custom HID Demo Urgent

Posted on August 15, 2011 at 02:27Hi everbody, I am using Custom HID Demo for stm32f107 eval board and HID demonstrator application. When application starts, Vendor ID and Produst Id appear. I wonder these : 1. Is Vendor ID fixed for each STM32 Cort...

irmakci by Associate II
  • 2630 Views
  • 7 replies
  • 0 kudos

Configuration USB ports HS in FS mode

Posted on August 12, 2011 at 10:10Hello,I am working on USB applications on a STM32F207IG. The usb communication works in FS with the port PA9, PA11 and PA12, in HS with the ULPI. But I need to USE the ports PB13 (Vbus) , PB 14 (DM) and PB15 (DP). T...