cancel
Showing results for 
Search instead for 
Did you mean: 

Configuration USB ports HS in FS mode

guillaume
Associate
Posted on August 12, 2011 at 10:10

Hello,

I am working on USB applications on a STM32F207IG. The usb communication works in FS with the port PA9, PA11 and PA12, in HS with the ULPI. But I need to USE the ports PB13 (Vbus) , PB 14 (DM) and PB15 (DP). They are HS pins configured in FS mode.

Here how I configured these pins:

RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOB, ENABLE ); GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; //Configure VBUS DM DP Pins GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_Init( GPIOB, &GPIO_InitStructure ); GPIO_PinAFConfig( GPIOB, GPIO_PinSource13, GPIO_AF_OTG2_FS ); // vbus GPIO_PinAFConfig( GPIOB, GPIO_PinSource14, GPIO_AF_OTG2_FS ); // D- GPIO_PinAFConfig( GPIOB, GPIO_PinSource15, GPIO_AF_OTG2_FS ); // D+ RCC_APB2PeriphClockCmd( RCC_APB2Periph_SYSCFG, ENABLE ); RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE );

Unfortunatly, it is not working. Can you help me ?

Thank you.

#stm32-usb
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
guillaume
Associate
Posted on August 16, 2011 at 08:55

Does anybody see what's wrong ? I really need help. Please.

loeffel2
Associate III
Posted on August 23, 2011 at 15:35

Hi

I also tried to use the OTG_HS periphery in device FS mode (internal FS Phy ) with the ST USB library ( STM32F205VB). The device example code does the equvalent pin initialisation as was shown in the erlier post. But there seems to be a problem with the VBUS pin (BP13) initialisation. If I define the VBUS pin as push pull and select the alternat function. The current flowing into the VBUS pin is 45mA or more. I guess the pin is configured as OTG_HS_ULPI_D6. Does anybody know how to connect the PB13 to the OTG_HS VBUS functionality?

regarsd Raphael

Posted on August 23, 2011 at 15:50

Does anybody see what's wrong ? I really need help. Please.

Perhaps you want to put this line before you remap it?

RCC_APB2PeriphClockCmd( RCC_APB2Periph_SYSCFG, ENABLE );

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
loeffel2
Associate III
Posted on August 24, 2011 at 14:04

Hi

I fugured out, what the problem was. It was a initialisation probelm of pin PB13 (VBUS) and a hardware problem of our board.

The initialisation of PB13 which seems to work for me looks like this:

   // Enable GPIO clocks (note: done at Gpio.c)

    //RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB , ENABLE);

    // Init USB DN and DP pins

    GPIO_InitStructure.GPIO_Pin = PB_USB_DN | PB_USB_DP;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    // Connect pins to alternate function

    GPIO_PinAFConfig(GPIOB, GpioPinNumGet( PB_USB_DN ), GPIO_AF_OTG2_FS);

    GPIO_PinAFConfig(GPIOB, GpioPinNumGet( PB_USB_DP ), GPIO_AF_OTG2_FS);

    // Init USB VBUS pins (note: has to be defined as GPIO_Mode_IN instead of GPIO_Mode_AF)

    GPIO_InitStructure.GPIO_Pin = PB_USB_VBUS;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;    

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    // Connect pins to alternate function

    GPIO_PinAFConfig(GPIOB, GpioPinNumGet( PB_USB_VBUS ), GPIO_AF_OTG2_FS);

    // Enable OTG_HS clock

    RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE) ;

Defining PB13 (PB_USB_VBUS) as input instead of alternate output solved the current flowing into this pin.

An injection current which flowed through an ESD diode to PB13 leaded to an instable sensing of VBUS.

regards Raphael