STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FatFS SDIO DMA write speed

Posted on July 23, 2014 at 14:28Hello.I'm trying to get more SD card write performance with STM32F207ZET6 + SDIO + DMA + FatFS.I'm using Kingston 8GB MicroSDHC 4 class. I formatted it with SD Formatter tool. File system FAT32 with 32KB clusters.Writ...

pbox by Associate II
  • 4393 Views
  • 5 replies
  • 0 kudos

USB library stalls while waiting for response

Posted on July 21, 2014 at 20:25 Hello, I'm currently working with an STM32F215 mcu and I'm attempting to write a test program with the USB-Host-Device Library V.2.1.0. The goal of this test project is to program the STM32F215 as a host c...

STM32CubeMX for F4 PolarSSL

Posted on July 17, 2014 at 23:10I've installed STM32CubeMX to see how it would work for a new board I'm planning on building.  Is there anything special I have to do to make PolarSSL show up in the middleware section?  I see LWIP, and can enable it,...

jwormsley by Associate III
  • 949 Views
  • 2 replies
  • 0 kudos

STM32F4 Cube and FreeRTOS Don't Cooperate

Posted on June 16, 2014 at 21:08Hi, I'm having a very difficult time getting FreeRTOS v8 to run with CUBE/HAL. I started out using CUBE to generate a basic example for an ADC input configuration, and a timer that will count up (or down) and execute ...

groufosse by Associate II
  • 1294 Views
  • 2 replies
  • 0 kudos

Can't find USB Host library for STM32 F3 series

Posted on July 10, 2014 at 06:59Hi - been checking for a while now, but I can't find any ''USB Host'' library for STM32 F3 series (I'm specifically using STM32F303VC and I have a STM32F3Discovery board).I only found: ''USB Device'' for F3 included...

maggie by Associate III
  • 1675 Views
  • 4 replies
  • 0 kudos

STM32F407 USB Disconnect detected interrupt problem

Posted on July 15, 2014 at 07:22Hi,I am presently working on STM32F407 USB, for my understanding i am referring the RM0090 Reference manual.In that manual for USB OTG FS, Global interrput register (GINTSTS) 29 bit as DISCINT bit at there they given ...

chandu1 by Associate II
  • 1076 Views
  • 1 replies
  • 0 kudos

HAL Timer Module - read & set counter value

Posted on July 16, 2014 at 12:22In the old standard drivers, you could use TIM_GetCounter(TIM2) and  TIM_SetCounter(TIM2, 0) to read or modify the timer counter values. Is there a similar thing within the HAL drivers? I can't seem to find any replac...

rajpaged by Associate II
  • 6260 Views
  • 1 replies
  • 0 kudos

STM32 Cube Download error

Posted on July 15, 2014 at 15:53Hi, i have errors on downloading the CUBE zip files, for F0, F2, F3.. I tried many times in previous days, but i reach only 90% of the files. Also within the CUBE environment, when downloading the .zip file i have an ...

mmedici by Associate
  • 1141 Views
  • 2 replies
  • 0 kudos