STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 USB FS Channel Halt problem

Posted on July 26, 2014 at 07:36Hi,Presently i am working with STM 32F407 USB FS, when i was writing some data into the channel then automatically  channel disable bit set in to the channel characteristic register and channel transmission interrupt ...

chandu1 by Associate II
  • 726 Views
  • 0 replies
  • 0 kudos

uSD card + board power off + prevent data loss

Posted on July 23, 2014 at 04:28I'm using STM32F4-Discovery for data/debug logging on uSD card. I have found samples in STM32Cube package:..\STM32Cube_FW_F4_V1.3.0\Projects\STM324xG_EVAL\Applications\FatFs\FatFs_uSDI ported this sample to my project...

harinath by Associate III
  • 1636 Views
  • 3 replies
  • 0 kudos

Calling the STM32 SystemMemory Bootloader

Posted on February 03, 2014 at 16:53I'm trying to launch the SystemMemory Bootloader on a STM32F4 as documented in this video: http://www.youtube.com/watch?v=cvKC-4tCRgw The PC detects a new device on USB but it does not enumerate. Using the Boot0 p...

Usb hid host problem

Posted on July 21, 2014 at 23:15I am interfacing a standard usb keyboard with stm32f4 discovery board. I am using a usb host library which are provided by st. Now the keyboard is successfully connected with discovery board and all keys are decoded s...

FatFS SDIO DMA write speed

Posted on July 23, 2014 at 14:28Hello.I'm trying to get more SD card write performance with STM32F207ZET6 + SDIO + DMA + FatFS.I'm using Kingston 8GB MicroSDHC 4 class. I formatted it with SD Formatter tool. File system FAT32 with 32KB clusters.Writ...

pbox by Associate II
  • 4375 Views
  • 5 replies
  • 0 kudos

USB library stalls while waiting for response

Posted on July 21, 2014 at 20:25 Hello, I'm currently working with an STM32F215 mcu and I'm attempting to write a test program with the USB-Host-Device Library V.2.1.0. The goal of this test project is to program the STM32F215 as a host c...

STM32CubeMX for F4 PolarSSL

Posted on July 17, 2014 at 23:10I've installed STM32CubeMX to see how it would work for a new board I'm planning on building.  Is there anything special I have to do to make PolarSSL show up in the middleware section?  I see LWIP, and can enable it,...

jwormsley by Associate III
  • 941 Views
  • 2 replies
  • 0 kudos

STM32F4 Cube and FreeRTOS Don't Cooperate

Posted on June 16, 2014 at 21:08Hi, I'm having a very difficult time getting FreeRTOS v8 to run with CUBE/HAL. I started out using CUBE to generate a basic example for an ADC input configuration, and a timer that will count up (or down) and execute ...

groufosse by Associate II
  • 1281 Views
  • 2 replies
  • 0 kudos

Can't find USB Host library for STM32 F3 series

Posted on July 10, 2014 at 06:59Hi - been checking for a while now, but I can't find any ''USB Host'' library for STM32 F3 series (I'm specifically using STM32F303VC and I have a STM32F3Discovery board).I only found: ''USB Device'' for F3 included...

maggie by Associate III
  • 1653 Views
  • 4 replies
  • 0 kudos