STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32cubeL0 loop in USART IT

Posted on September 11, 2014 at 17:54Im using STM32Cube_FW_L0_V1.1.0 on a STM32L052C8T6 Why there is some loops into TX and RX IT functions? For example: in  UART_Receive_IT() At the end of the reception there is: while(HAL_IS_BIT_SET(huart->Instanc...

gwendal by Associate
  • 2395 Views
  • 5 replies
  • 0 kudos

STM32L0xx LPTIM with STM32L0CUBE

Posted on October 28, 2014 at 06:58Hello,I have some problems to initialise the Low power timer correctly. I'm using the STM32Cube firmware and a STM32L053R8 chip. To start with the LPTIM, I will only toggle a GPIO but I'll never enter the interrupt...

thierry2 by Associate
  • 836 Views
  • 0 replies
  • 0 kudos

dual bank boot STM32F437 vs STM32F439

Posted on October 24, 2014 at 16:14Hi,I am using a STM32F437 and need to use the dual bank boot feature to perform live firmware updates. I have the boot0 pin tied to ground.According to the Reference Manual:In STM32F42xxx and STM32F43xxx devices, w...

graffiti by Associate III
  • 1831 Views
  • 2 replies
  • 0 kudos

stm32f429 Disco direct to VGA Monitor

Posted on October 09, 2013 at 15:35Hello :) I just remove the LCD from one of my board and made a R2R Resistor DAC connected to the LCD dedicated pin. The only pins you need are the 3 x 6bits colors , the vsync , hsync and GND. After some changes in...

warcatz by Associate II
  • 4930 Views
  • 7 replies
  • 0 kudos

USB <-> MIDI STM32F103

Posted on October 20, 2014 at 20:40Hello! Need source code or examples for implementations USB <-> MIDI STM32F103. #midi #usb #stm32f103

swing82 by Associate II
  • 2884 Views
  • 4 replies
  • 1 kudos

STM32F407VG Bootloader via USART3

Posted on October 23, 2014 at 16:37Hello All,We are using STM32F407VG & are having issues with bootloader via USART3 PC10/PC11. From the SW, we see that the processor is entering the bootloader mode.When 0x7F is send, the processor responds with ''0...

pramuka by Associate II
  • 1645 Views
  • 2 replies
  • 0 kudos

usb bulk transfer

Posted on October 23, 2014 at 11:29before i was using pic18f2550 for usb connection on our product, now i decided to use stm32f4 anymore. but i couldnt find any simple usb bulk example (except cdc,hid). i am hardware engineer not software expert. i ...

mrjaner by Associate II
  • 3518 Views
  • 2 replies
  • 0 kudos

STM32Cube CDC new Endpoint

Posted on October 21, 2014 at 08:53I creat new USB CDC project and add new IN Endpoint (0x83). I correct USBD_CDC_TransmitPacket for new Endpoint (0x83). Yet data transfer not working. What should I do to my IN Endpoint (0x83) worked? #stm32cube ...

z1060 by Associate II
  • 1908 Views
  • 4 replies
  • 0 kudos

STM32F2xx USB VCP firmware example

Posted on October 17, 2014 at 10:04May I know where can I get the firmware example for STM32F2xx for USB Device VCP???I tried this link, but the firmware is not working, the USB doesnt emurate!https://github.com/suapapa/stm32_library/tree/master/Pro...

ho by Associate II
  • 2777 Views
  • 7 replies
  • 0 kudos

USBD_DeInit does nothing? How can I turn off USB?

Posted on October 16, 2014 at 20:44I have the code for USB device working.  I initialize USB with USBD_Init.  My code also  needs to turn off USB completely in one mode to minimize power consumption.  I tried USBD_DeInit.  There was no change in the...