STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lwip on E407 board, source for STs AN3966

Posted on January 13, 2015 at 23:40Hi all, I want to run lwip on the Olimex E407 board. STs AN3966 seems to be a good start, but I cannnot find the ST modifications auf the software. It is not in the download from http://savannah.nongnu.org/projects...

detlef by Associate
  • 1725 Views
  • 2 replies
  • 0 kudos

STM32F105 eeprom simulation

Posted on January 13, 2015 at 10:27 Hello I am try write a configuration in a microcontroller STM32F I am using stsw-stm32010 code base example. The example work properly. But when I make my code don't work. I want...

lemac by Associate III
  • 1159 Views
  • 1 replies
  • 0 kudos

STM32CubeMX + MDK-ARM: using UART

Posted on November 25, 2014 at 01:16Hi All,I'm just starting up on development for STM32 Cortex M0 and M4, trying to use the CubeMX with MDK ARM to develop a simple communication protocol over rs485.However I could not find confirmations for my ques...

balazs by Associate II
  • 1078 Views
  • 1 replies
  • 0 kudos

Update co-processor FW via USART

Posted on January 11, 2015 at 10:59This is probably a too-broad question, but here goes:I have a system where a master MCU (STM32F103) communicates with another MCU (TI CC2540) via UART. The master can be connected to a PC via USB.The task at hand i...

boaz by Associate II
  • 1227 Views
  • 1 replies
  • 0 kudos

CubeMX 407s USART/UART inconsistancy

Posted on December 12, 2014 at 22:31I'm working on a system where we use a STM32F407VGT6. I set up the project in CubeMX (latest version). We are using USARTs 1,2, and 3 with interrupts for receive.I'm having some issues with the USART portion of th...

STM32F205 USB core reset for close port

Posted on January 05, 2015 at 14:24Hello.I am using stm32_vcp_1.3.1 stack for USB OTG. I have a problem when the USB connection to the PC is ended because App kill (no interrupt to tell me about it). I found that I stay in a loop of OTG_FS_IRQHandle...

Barbie by Associate II
  • 1750 Views
  • 3 replies
  • 0 kudos

stm32f429 Discovery vcp with STM32CubeMX drivers?

Posted on December 22, 2014 at 07:06Hello, Does anybody have a working vcp (usb cdc) project on a STM32F429 Discovery board using the stm32cubemx(hal) drivers? If so, could you send it to me? Just trying to get Windows 7 to recognize the vcp. I crea...

renasis by Associate II
  • 1343 Views
  • 2 replies
  • 0 kudos