STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F42x ROM DFU Descriptor

Posted on March 30, 2015 at 11:32It appears that DFU in the STM32F42x ROM Bootloader has an issue: The device returns a descriptor response string as a malformed packet (according to wireshark) for the @Internal Flash interface. The bLength field in...

Multiple funcs mapped to one Pin

Posted on March 29, 2015 at 00:45Hi,     I am a student studying EE, and do not have any experience in circuit design besides the theory being taught in college and a six month hardware design Co-Op. Currently, I am developing a board to be used for...

ziegler by Associate
  • 1522 Views
  • 3 replies
  • 0 kudos

SPL to CubeF4 conversion issues

Posted on March 27, 2015 at 12:22I need to integrate an old code written using the Standard Peripheral Library to a new (big)project that's using CubeF4.As easy as it sounds I can't find any commonality between the libs..1. Is there any documentatio...

ariel2 by Associate II
  • 1962 Views
  • 4 replies
  • 0 kudos

USB Device on STM32F405, lost bytes SOLVED!

Posted on March 27, 2015 at 12:07After updating to version 4.7.0, the error appears no more. I'm back to version 4.6.0 and the error will also no longer occur. Now I'm not sure what it was. Maybe a Windows effect (Shut down the PC and start again), ...

rm2399 by Associate III
  • 993 Views
  • 1 replies
  • 0 kudos

STM32F103 Bootloader Branching Troubles

Posted on March 25, 2015 at 02:45I've read just about all the existing posts regarding jumping from one code section to another and still I cannot jump without triggering a hard fault. I'm adhering to advice given such as always jump to an address w...

Single Library for USB on all STM32 devices?

Posted on October 19, 2012 at 13:18I'm developing some software for multiple STM32 devices. One of the features it needs is a USB Virtual COM port.I've developed a version that works with USB VCP on the STM32F103 using this library:stm32_usb-fs-devi...

gw by Associate II
  • 2742 Views
  • 7 replies
  • 0 kudos