STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Device s/w hang during USB Disconnect

Posted on April 28, 2015 at 13:56Hi All,Hi, I am using the STM32F407IG microcontroller. I am using the USB HID example provided by ST. This code is configured to make USB as USB Device and Self Powered rather than bus powered. In our board since th...

Switching/selecting ADC source

Posted on April 26, 2015 at 19:36 I am using Cube generated code, exported to EWARM, running on a Nucleo L053R8 board. My question is how to select the active ADC source outside of the ADC initialization code. For instance, with channel 12 and 13...

joe2399 by Associate II
  • 3037 Views
  • 8 replies
  • 0 kudos

handling Boot0 floating input

Posted on April 22, 2015 at 22:03Hello,Unfortunately, we've manufactured a large batch of boards with the STM32F103's BOOT0 pin left floating, and not pulled high or low.  As a reliable fix (besides soldering jumper wires) for this issue, can the Bo...

brianj by Associate II
  • 6240 Views
  • 11 replies
  • 0 kudos

USB communication between 2 microcontrollers

Posted on April 23, 2015 at 20:26I have a smt32f3discovery and with him I want to create a ''virtual USB host'' in order to access the endpoints of the other controller. I wonder if this is possible or is there any code or library written for it or ...

esovo1 by Associate II
  • 999 Views
  • 1 replies
  • 0 kudos

STM32F4 Processor Load

Posted on September 19, 2014 at 04:43Hi, Is there a way to measure CPU load on the device? Using IAR EWARM 7.2 if that makes any difference. I did a search but could find anything. The usual cryptic Google returns to adwords. 8--) #freertos #prof...

STMCubeF0 v1.2.1 and CMSIS Drivers question

Posted on April 17, 2015 at 13:06Hi all,I've just downloaded STM32Cube_FW_F0_V1.2.0 and applied latest patched to upgrade is to V1.2.1. I was expecting it to be fully CMSIS compliant, so for example I could use CMSIS compliant USART interface. So I ...