STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB CDC - Issue with size buffer in EP0 OUT

Posted on August 28, 2015 at 17:09Hello everybody,I'm using USB CDC in my project with STM32L151CC, and I got little issue with the USB Library.I know that the MAX SIZE of EP0 buffer to transmission is 64 bytes.In my debugs, I could send 1 byte, 2 b...

uilter by Senior
  • 696 Views
  • 0 replies
  • 0 kudos

STM32F070 USB not working

Posted on August 28, 2015 at 11:06Hi. I am using STM32F070CB with libraries STM32F10x_L1xx_F3xx_USBL(v4.0.0) and STM32F0xxSPL(v1.1.0) to implement custom HID to implement simple hello world(PC sends 64 bytes and MCU sends back the same 64 bytes)The ...

stm32f042 can problem

Posted on August 27, 2015 at 09:41 void HAL_CAN_MspInit(CAN_HandleTypeDef* hcan) { GPIO_InitTypeDef GPIO_InitStruct; if(hcan->Instance==CAN) { /* USER CODE BEGIN CAN_MspInit 0 */ /* USER CODE END CAN_MspInit 0 */ /* Peripheral clock en...

STM32L053-Nucleo board's RTC not running.

Posted on August 25, 2015 at 06:52Hello, I have implemented RTC on STM32l053-Nucleo using CubeMX and CubeL0 HAL libraries. I set and get the time and date in RTC using HAL functions but the RTC is not running, I am getting the same time and date I h...

salman2 by Associate II
  • 1475 Views
  • 1 replies
  • 0 kudos

STM32F4 USB Endpoint question

Posted on August 14, 2015 at 09:35Hi! I used CubeMx to generated USB HID Device example code and  update to F4_Discovery Kit.The default endpoint address is 0x01 and 0x81. I could send data from PC to STM32F4 via USB. and STM32F4 also could send dat...

STM32 bootloader form SD card

Posted on August 21, 2015 at 09:04 Hello ! I have a problem with my bootloader form SD card. I think i try everything, now i don't have any ideas. App in sd card have changed memory start address to 0x08002000 and memory size to 0x0003E000. ...

piotr2399 by Associate II
  • 3332 Views
  • 8 replies
  • 0 kudos