STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STm32F USB VCP example

Posted on March 10, 2015 at 16:12 I am building a microcontroller based on the STM32F302K8 chip and I am trying to send data to host PC via USB. My echo code below based on an example in the forums works: static int8_t CDC_Receive_FS ...

B Zikhali by Associate III
  • 4680 Views
  • 11 replies
  • 0 kudos

View Trace with Eclipse

Posted on October 29, 2015 at 10:28 Hi, I'm new to STM32 and I got a STM32F7 Discovery Board. I'm playing around with the USB Host MSC Standalone Application example provided in the STM32Cube_FW_F7 package. In the Application, th...

merelda by Associate
  • 754 Views
  • 0 replies
  • 0 kudos

How can i Ethernet communication with STM32F4

Posted on October 27, 2015 at 21:14I am planing a project.Maybe his project will contain UDP communication.Can I use STM32F4 or other Stm32 product.When I am looking for similar project,i found working on localhost (as 127.0.0.1).But i want  sending...

STM32 HAL UART Error managment

Posted on October 12, 2015 at 17:27Hi All,i have a problem with the managment of the UART Error.Particularly when the error occurs in ''HAL_UART_ERROR_ORE'', the device is locked and I can not clear the error.I tried using the following instructions...

mgualdi9 by Associate II
  • 4481 Views
  • 6 replies
  • 0 kudos

reliability of OTG USB on stm32f4 Disco

Posted on September 07, 2015 at 09:51 I am intending to port GRBL Gcode interpreter to run on stm32f4 discovery and I have seen several reports that the OTG USB port ( more specifically the provided ST firmware ) is not reliable. A colleague in the...

estie by Associate II
  • 1995 Views
  • 5 replies
  • 0 kudos