USB OTG FS host channel interrupt is coming up abnormally too many times.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-10-26 1:23 AM
Posted on October 26, 2015 at 09:23
i m using stm32 Cube mx codes for USB OTG FS host.
with most pendrives, the host channel interrupt and RX queue level interrupt is coming normally, around 20-25 times during mass storage class initialization. but with few pendrives, the the host channel interrupt is as high as 29000+ (it worst value while using kingston 8gb pendrive) while rx queue level interrupt is low as 30-40 times max.i wonder why hs channel interrupt is coming so many times as for 1 data packet transfer, it should be called only once. and as i have went through the code, we are communicating with pendrive around 19-20 times during mass strorage class initialization.so my question is... why with kingston pendrive i am facing this issue?? is it because interrupts are not handled properly?? #full_speed #host_class #usb
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0